AXIS#.VL.VFTHRESH

Description

This parameter reports the overall overspeed fault threshold. The following thresholds with the smallest value is used as the overall overspeed fault threshold:

  • User overspeed threshold (AXIS#.VL.THRESH).
  • Motor mechanical overspeed threshold (1.2 x AXIS#.MOTOR.VMAX)
  • If AXIS#.MOTOR.TYPE = 6, the motor back EMF overspeed threshold ((1.02 x 1000 x VBUS.OVFTHRESH) / (AXIS#.MOTOR.KE x sqrt(2))).

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

N/A

Range

N/A

Default Value

N/A

Data Type

Float

Stored in Non Volatile Memory

No

Variants Supported

All variants are supported.

Related Topics

Velocity Loop | AXIS#.VL.THRESH | AXIS#.MOTOR.VMAX